Part Number: INA333
We have has several INA333's fail on us where they are no longer outputting voltage and vcc to gnd is low resistance when using the same topology.
Two potential things we are violating in the datasheet.
1. I can't seem to find a max output current spec for this amp. We have the output going through a lowpass r=10ohm and c= 330pF filter before it hits an ADC. Could the parts be failing because every turn on the cap briefly pulls 0.120 A to charge from zero? We could increase R to prevent this but the datasheet says something bogus like Absolut Max rating: Output short-circuit = Continuous for both min and max?
2. Our Vin+ terminal comes up before the V+ and V- Rails supply power to the chip. The inputs are current limited to a milliamp and the input to the ina333 should be high impedance so I don't think this would be an issue.