Hello together,
can I suplly the OPA196 with a normal 9 V Battery, or I have to consider anything?
Do I have to restrict the supply current general?
Thanks for helb,
Marvin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello together,
can I suplly the OPA196 with a normal 9 V Battery, or I have to consider anything?
Do I have to restrict the supply current general?
Thanks for helb,
Marvin
Hello user5990299,
The OPA196 certainly can easily be powered by a single 9 V battery. You shouldn't have to provide any sort of current limiting circuit because the OPA196 operating current alone is very low; at most 250 uA. Any load you drive with the OPA196 will require current be sourced or sunk from the op amp output. That load current originates from the 9 V battery and flows from/into one of the OPA196 supply pins.
Just exactly how much current the OPA196 can provide is limited and function of the output stage electrical characteristics and operating temperature. The OPA196 datasheet Typical Characteristics graphs in Figures 6 and 7, Output Voltage Swing vs Output Current, provide a good representation of just how much output current can be expected from the OPA196. Normally, a precision op amp such as the OPA196 is used to drive a light load such as 10 kilohms, or 2 kilohms, and the output current is low. A 9 V battery can easily handle that total operating current and output load current.
Make sure that the OPA196 is being operated within its linear common-mode input voltage range, and linear output voltage swing range. If the op amp is biased in such a manner that the output is up against one of its swing rails, it won't be in its linear operating range and the voltage offset will be outside its specified range. It would be helpful if we could see your test circuit as Kai mentioned.
If you would like some help with understanding the voltage offset of an operational amplifier, have a look at the TI Precision Labs - Op amps series, Section 2. I think that may be help you with your voltage offset measurement:
https://training.ti.com/ti-precision-labs-op-amps
Regards, Thomas
Precision Amplifiers Applications Engineering