This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO122: Isolation amplifier

Part Number: ISO122

Dear sir, please help

I need isolation amplifier (follower)  to transfer 1...2V DC voltage. I have two unipolar power supplies +5V-1 and +5V-2.  These power supplies isolated from each other.  Can I use ISO122?   Can you recommend another amplifier?

TIA

Sincerely,

Vladimir Naumenkov

www.agat.by