Part Number: INA302
Hi,
We have implemented INA302 for over current protection in our design.
The LIMIT2 is set for 40A current limit. The LATCH2 pin is tied to GND (Transparent mode)
The Delay pin has been connected to a 10uF capacitor to provide 2.44s delay.
If there is a surge current exceeding 40A (say for 100us), our expectation is that ALERT2 signal should not be asserted as we have set a time delay of 2.44s.
But what we observe is that the ALERT2 is asserted after 2.44s even though the surge current doesn't exist beyond 100us.
We have replaced the IC and find the same behavior with the new IC as well.
Is this the expected behavior of the IC? if yes, then what is the purpose of the Delay?
Thanks,
Yogesh M R