Part Number: OPA548
Hello,
I am using an OPA548 to drive 5Hz 1Apk signal into a 7.05ohm, 4.52mH RL load as shown. The E/S pin is on the output of a normally-open opto-relay for enable/disable control. After the part heats up a bit (tab of the package reaches around 104degC), the output begins to disable and re-enable in 15-30ms spurts around the peaks of both the positive and negative cycles. It continually gets worse until every cycle disables/re-enables as it gets hotter.
I verified that the E/S pin is toggling to disable/re-enable the output, and it is not being commanded to do so.
My question is if this part is damaged, or is this normal behavior? A 30ms dropout seems suspect for thermal shutdown, as the datasheet specs the output will not re-enable until die temp drops back to 140deg. If this part does appear to be damaged, could this be due to disconnecting the load with the output still enabled? Could this cause a large current spike that would damage the part? Or instability? Any help would be appreciated.
Thank you,
William