Hi,
We are using TLV2371DBVR and OPA2364 opamps in our design.
I would like to know if the Output of the Op-Amp can withstand ESD test according to IEC 16000-4-2 standard, which is +/- 4000V Contact charge and +/- 8000V Air Discharge. Output of the Op-Amp directly connected to pin without any components in series or parallel.
What will be the way to protected Output of the Op-Amp or is there Different Op-Amp Certified with IEC 16000-4-2 Standard?
Jitsu Patel.