This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi dear supporting team,
how about the max operating Tj of LM7301? from 85degree TA, it seems Tj could not exceed 100 degree. customer is operating at 8V, they normally get 96degree case temp. and the highest case temp could get to 110degree. is it ok? tks a lot!
hi Paul,
tks for reply!
because it is in the power module, they are hard to measure the ambient temp, the only temp they could measure is the case temp. so for 110degree case temp, is it over the operating range? tks!
Hi Vera,
Take a look at the TIPL video on temp and power: training.ti.com/ti-precision-labs-op-amps
In this case, the equation used would be: Tj = Pd*(Theta_JC)+Tc
Just accounting for the quiescent current of the device at 8V supply of 0.6mA for Pd, the junction temperature with a case temp of 110° C would be:
DBV Package: (0.6mA)(8V)(122 °C/W)+110°C = 110.6° C
SOIC Package: (0.6mA)(8V)(65 °C/W)+110°C = 110.3° C
If the output voltage is known, you should add that to the power dissipation of the op-amp. To violate the absolute maximum with a 110°C case temperature, the circuit would need to be dissipating 327mW in the DBV package or 615mW in the SOIC package.
Hope that helps,
Paul
Hi Paul,
yes, I know that equation. my question is: what's the max Tj for normal operation without violate the d/s spec? for 150degree, it is Tj that without destroy the chip, but if approach to 150degree, the spec should be degraded a lot. isn't it?
Hi Paul,
In this calculation, you still use 150 degree which is the absolute rating. But If use my calculation, it seems the operating TJ could get to 155degree. Could you double check that with 150 TJ the chip could work within the d/a spec? Tks!
Hi Paul,
so if customer only operate at 8V, if they get 96 degree case temp for normal, and max case temp will go to 110degree. will this violate the operating rating? I am wondering could we use 150degree as the operating temp. tks!