Other Parts Discussed in Thread: TINA-TI, ADS1278, , THS4521, THS4551, TL072, THS4521EVM
Tool/software: TINA-TI or Spice Models
Hi There
I have a low frequency (say 10Hz) differential input signal coming from a sensor centred around 1.65V and swinging down to 0.3V and up to 3V
The intent is to buffer this with a unity gain differential buffer and feed into a ADS1278 ADC. I'm hoping to use the THS4521-HT to do this (its a high temp application), my supply rails will be 0V and 3.3V
In terms of the output voltage swing of the THS4521-HT it can go down to 0.09V and upto 3.11V (typ at 125 degrees), this should be fine for my application.
In terms of input common mode limits, i'm unsure if its my calculations / understanding or the Tina Spice model for the THS4521.
Having read tech note "Analysis of fully differential amplifiers" and watched the training video "
16.2 TI Precision Labs – Op Amps: Fully Differential Amplifiers – Input and Output, Common-Mode and Differential-Swing Analysis"
using both these methods (see pic below) i get a input common mode of 1.65V. (gain of 1, sensor common mode and the output common mode 1.65V.
So my understanding there is no AC (peak to peak) component to worry about for the input common mode voltage for a fully differential input and output configuration?
so therefor 1.65V is within the limits of the THS4521-HT specs (0-1.8V for a 3.3V supply)
However when i simulate the following circuit it works with the model i got from another post and edited (https://e2e.ti.com/support/amplifiers/f/14/p/530720/1931878?tisearch=e2e-sitesearch&keymatch=THS4521%20common%20mode#1931878
Tina file here (with the working op amp - replace with website model to see distortion)
Basically i want to know if
1) is there a problem with my understanding or is there a problem with the tina model on the website?
2) if its my understanding any suggestions of how to interface the signal at the top to the ADC1278?
Kind Regards
Martin