Part Number: XTR110
Other Parts Discussed in Thread: OPA2350
Hi all,
I am using the XTR110 as 0-5V to 4-20ma wired according to the device datasheet, page 6, having the pin5 as input and pin 3 to GND.
I am using the VP0808L mosfet transistor and everything is running well.
When I change the transistor with the ZVP4525GTA, i get a damaged XTR110 immediately after power on the circuit.
Same if I use the FQT2P25TF.
Looking more carefully at the damaged units, having replaced the testing transistors with the trusted VP0808L I measure
V(pin1)=V(pin13)=V(pin14)=Vcc=+22V
V(pin10)=0
which tells me that internal opamp A1 is damaged....
My RL=312Ohm, V(pin5)=2.5V and, Vcc=+22V
Any ideas for the cause of damage?
Any suggestions for an alternative transistor, having better power dissipation than the VP0808L?
Thanks
Nick