Part Number: LMP2012QML-SP
Other Parts Discussed in Thread: LMP2012, LMP2011
Hello
Is there a P-SPICE model for simulating the output change according to the temperature change in the below device?
LMP2012QML-SP
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMP2012QML-SP
Other Parts Discussed in Thread: LMP2012, LMP2011
Hello
Is there a P-SPICE model for simulating the output change according to the temperature change in the below device?
LMP2012QML-SP
Best regards.
Hello Louis
The LMP2011 pspice model can be applied to the LMP2012. It is just a single channel version.
The pspice models do not have variations for temperature. On an op amp, on many crictical parameters such as input offset voltage, the change over temperature is not predictable, making it impossible to model.