Part Number: INA240
Other Parts Discussed in Thread: TIDA-00909
Hi ,
How much is the enough slew rate and bandwidth of current sensors in FOC algorithm for:
1)Inline current sensing
2)low side current sensing
Regards, Mohammad
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA240
Other Parts Discussed in Thread: TIDA-00909
Hi ,
How much is the enough slew rate and bandwidth of current sensors in FOC algorithm for:
1)Inline current sensing
2)low side current sensing
Regards, Mohammad
Hi Mohammad,
It is not FOC algorithm that determines current sensing speed requirements, nor does it have much to do with the location of the current sensor. The requirement for the current sensor is largely determined by the motor itself(#of poles), how fast (RPM) you spin it and how accurate you want the current sensing to be in all load conditions.
Ultimately, it comes down to how much time the current sense amplifier has to settle after each PWM transition. Consider the worst case duty cycle and it determines how fast an amplifier you’ll need.
Regards, Guang
Hi Mohammad,
Can you please post related questions to the same thread and not opening new thread for each? Please click on “this resolved my issue” to close the other thread if you decide to abandon it.
Regards, Guang
Hi Mohammad,
I’ll leave it to your to look into the relationship among motor speed, poles and PWM switching frequency. There are online documents/pages you can refer to, such as this one. http://www.ti.com/lit/an/slyt692/slyt692.pdf
The PWM frequency determines how much time the current sense amplifier has to react to a change in current when cycle by cycle current control. With a 10KHz PWM and 50% duty cycle, the upper limit is 50uS. This is doable with almost all devices.
If the PWM becomes 50KHz, the upper limit for the settling time is now 10uS. In this case, you probably want to select that device that has a slew rate at least 1uS/V and can settle to a reasonable accuracy within a few uS.
Regards, Guang
Hi Guang,
Guang Zhou said:The PWM frequency determines how much time the current sense amplifier has to react to a change in current when cycle by cycle current control. With a 10KHz PWM and 50% duty cycle, the upper limit is 50uS.
TI has test the 240 in-phase monitor up to 100KHz PWM 50% duty via TIDA-00909. If I recall it compares 50% PWM duty cycle via scope captures 40KHz - 100KHZ. That hooked this fish easily until later discovering the modulation used was specialized Space Vector PWM reference SPRA524.
Hi,
You can still have large current in the motor under no load conditions, where the speed will increase. When loaded, the speed will decrease and torque will increase if you keep the current constant.
You’re correct however, there are situations where the duty cycle can be almost 0%, in a PWM modulated sinusoidal drive. The saving grace is that at any given moment only two phase currents are required in order to derive the motor speed and position information. If one phase is too difficult to measure, this information can be derived from the other two windings. However the current sense amplifier does determine the top PWM frequency. As a hypothetical example, if the CSA settles to 1% in 5uS, then the top PWM can never be more than 200KHz because at that point the CSA needs 100% of the duty time just to settle.
Low side or inline current sensing doesn’t make a big difference in terms motor control itself. However, in addition to motor safety and health information, inline sensing provides the direct winding currents which does reduce the amount of math the controller has to deal with.
Regards, Guang
Hi,
Since I haven’t heard from you in a while, I’m going to close this thread. Please post back if you have further questions.
Regards, Guang