Part Number: XTR110
Dear Technical Support Team,
My configuration of XTR110KU is following.
Vin: 0V~10V
Iout: 0mA~20mA
I adjust the offset pin(Volume register).Then almostdevice show 0mA(target is under 4.8μA) when Vin=0V after adjusting register(VR) of offset adjust pin(OK device).
However some device doesn't shows under 4.8μA in spite of adjusting offset pin(VR). It shows 5.6μA or 7.6μA or 8.0μA(NG device).
When replace the other device, it behave OK. It seems Individual difference of device.
I attached my schematic. Why is there difference between OK and NG?
Best Regards,
ttd