Other Parts Discussed in Thread: THS3001, THS3491, THS4271, THS4211, LM7171
Currently I'm using LM7372 in a design but the settling time is only specified to 0.1% for a 10V step, also noise is higher than I'd ideally like. Does TI have a suitable replacement for this part that has settling to 0.01% step in less than 70nS specified ? Also preferably with noise down in the 1 - 3 nV/RtHz region. I know ADI make such a part but wondered if TI had anything newer that would be worth evaluating ?