Other Parts Discussed in Thread: INA210, INA303, INA302, INA301, INA300, INA381
Hi Sirs,
Sorry to bother you.
I think it would be good if the Digital output can only provide HIGH/LOW signal instead of I2C.
Therefore, I found INA210~214 which may feet our application.
Our application is
The actual output current should be up to 75mA
And we would like to set the output as HIGH when the current is higher than 10mA and LOW when the current is lower than 10mA
Which one is suitable for our application between INA210-214? How should I select RL?
Please help to advise. Thanks.