Other Parts Discussed in Thread: LM331, TLC555
Hi Ti,
I am looking for a small footprint, quick-to-implement sinewave generator that meets the following condtions:
1. I have a 5V and +-12V power supply on my circuit, so the sinewave generator needs to be powered from these supply
2. Amplitude stability down to at least 0.1%
3. Frequency stability down to at least 1%
4. Ideally I would love to have the sine wave to reach 20V pk-pk, but I could have a gain if needed.
5. Low harmonic distortion but I don't really have a requirement for it.
6. Power budget is now really a concern
7.
If the surface mount sine-wave generator/ function generator requires SPI/I2C communications for setup, it would be really helpful to have available programming code/examples.
Thank you and I look forward to hearing from you soon,
Khoi Ly