Part Number: LM358
Other Parts Discussed in Thread: LM393
Hi folks.
I am trying to build a motor speed controller using labview. I got the labview diagram circuit but struggling with the motor circuit.
I am using Arduino uno and DAC (MCP4922). If i connect any component after MCP4922, the voltage drops dramatically. I want to make the motor operate according to the voltage, but it just working really slow.. I've used different motor to check if it is a motor problem, and i've measured the output voltage using digital multimeter- measuring directly from the DAC, i get the right voltage, but whenever i connect LM358(in above circuit i couldn't find the LM358 so just put it instead) or the diode, only few voltage comes out so the motor is not working according to the voltage we control. I think the problem is that too large current is taking through the motor and can not find the way out. Please tell me how i can make it work.