This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4244: Output impedance

Part Number: OPA4244


Dear all, 

I'm interested to have more information on the graph posted by Paul in the following thread  https://e2e.ti.com/support/amplifiers/f/14/t/786914

Can we consider Zo@DC equal to Zo@10Hz (=727,7 Ohms)? 

Could you please confirm that data are related to open loop output impedance? To get OPA4244 closed loop impedance is it correct to divide Zo(Aol) by the following factor: Aol/Acl? 

ex: @10Hz , op amp OPA4244 (Aol=106db) configured as a voltage follower (Acl = 1) then Zo(cl) is about 727,7/199526/1=0,0037Ohms. 

Thank you and best regards, 

Benoît,