Other Parts Discussed in Thread: INA210
Hi team,
When using INA199A-Q1 in DCDC for output current sensing after inductance with 0.1 mΩ sensing resistor,
1. in the case of small current, like 2-3A, the output has a few kHz (3.3kHz) oscillation.
2.When load on with 45A, output should be calculated as 225mV (with 50V/V gain), while the waveform is triangular wave with 13.5kHz frequency. Why it is triangular, the mid-point is ~225mV
Best Regards,
Gene