Part Number: LM13700
Hello TI Experts,
I'd like to use LM13700 to do the AGC part,from the datasheet,their is only simlified reference design,do we have complete design of LM13700 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Qianqian,
Figure 25 is a complete circuit. The automatic gain is based on this output current formula. VOUT = Iout * Rout
Larger input signals increase the 20uF cap voltage which increases Id current. Increased Id current reduces the gain. So this is a simple compression circuit to increases the dynamic range of input. So a wide input amplitude range becomes a more narrow output amplitude range.
More complicated circuits could record the peak voltage and use an error amplifier the get a fixed peak output voltage. The error amplifier would drive the Iabc current instead of diode bias pin. Loop stability and response time of the automatic gain become side effects to consider.
What is the expected input signal range (voltage & frequency)? Does the DC component of the input signal need to be preserved? What is the acceptable output voltage range?
Dear Ron,
Thank you very much for your kindly reply~`
Our shematic is as followed, it can achieve basic function, now the SNR is 70dB, is their any way to improve the SNR?
Another question, our target is :the input audio signal amplitude is 0.5v to 2V, and the output is 1V, do you have any suggestion to do this?
Qianqian,
Many LM13700 applications including this one run in an open loop (no feedback). Therefore it will naturally lack the S/N that high performance op amp will have. In negative feedback op amp circuits, the op amp uses some of its gain to perform the designed function. The remaining op amp gain is used to drive the difference input voltage closer to zero. This greatly reduces non linearities that will be present in the output signal. Conversely, LM13700 is open loop so nonlinearities become part of the signal with no reduction. It is the open loop that is the issue . Closing the loop (adding negative feedback) would fix the problem but it would also negate the variable gain feature of the LM13700.
In addition, the AGC function will also add distortion as the AGC function will have ripple at input frequency and will have distortion when it needs to correct the gain when the input signal changes.
Qianqian,
I simulated the figure 25 data sheet design. I did not like that input offset error was such a big factor that had to be corrected manually (with input potentiometer) . .So I added a DC input offset correction circuit (R4, C2, buffer IOP2) to eliminate pot, P1.
LM13700 Fig 25, Vos correction.TSC
Here is the gain compression chart . Vout peak vs. Vin peak
Note that the voltage drop of Darlington buffer changes with temperature so Vout vs. Vin results can vary across temperature.
0.5Vp to 2Vp is a 4:1 range. As is, the output is about 3.9Vp to 5.1Vp which is a 1.3:1 range.
How many channel do you need? How close to 1Vp do you need?
What is the range of the input frequency bandwidth needed?
Does the amplitude change slowly or rapidly?