Part Number: LM5056A
Other Parts Discussed in Thread: INA282, INA240, INA193, ADS1113, INA226
Dear Team,
The I2C read mode of the LM5056A is bit bank I2C is not a regular regular I2C. Dell said that their OS6 code does not support bit banks, so Dell asks us to find out if there is no pin to pin. If there is no pin to pin, please help recommend a suitable one.
I check on the TI.com website, it seems this one is the only solution to measure voltage up to 80V.
Because they use this device to measure 54V rail.
Or they need to use a different approach?
BR
Kevin