Other Parts Discussed in Thread: TCA9406, INA226, MSP430F5500
Hi,
We are using 3 INA3221's on our platform for bus/shunt voltage measurements. Out of 3, 2 Devices are working fine and giving out correct measurements (For one device A0 is connected to VDD 3.3v and for other device the A0 is connected to GND) both of these devices are connected to supplies between (0.7v to 2v). On the third, only 2 channels are in use ( channel 1 1.8v and channel 2 3.3v) we are unable to read anything from 3rd device.
The pullup on the I2C lines are 4.7k. Below is schematic
We also observed that when we try to observe the SDA signal on scope and probe (10Mohm 10pf) the resistor R875 (at end towards IC) we are able to read the registers and able to take voltage measurements. Speculating that probe is adding capacitance (10pf) and that capacitance is somehow effecting the bus. But we don't see anything mentioned in device document about capacitance requirement when A0 is connected to SDA.
Note: We are also observing this issue on other platforms which use 4 INA's where the problem is with devices where A0 is connected to SDA/SCL.