Hi Support team
AS D/S page 23, 9.2.2.3 Input Filtering mentioned,
Total effect on gain error can be calculated by replacing the 5-kΩ term with 5 kΩ – 30%, (or 3.5 kΩ) or 5 kΩ +
30%, (or 6.5 kΩ).
my customer just curious why the input impedance will have such higher tolerance about +/-30%?
if so, how about the internal divide resistor, is this part also has +/-30% tolerance?
for example, 3.5Kohm will match with 350kohm & 6.5Kohm will match with 650Kohm? am i correct?