Part Number: ISO124
Other Parts Discussed in Thread: ISO224
Hi team,
My customer is evaluating our ISO124. I noticed that in our datasheet, the maximum input voltage of the primary side is 100V. So when there is a transient voltage that is higher than 100V applied to the input, I assume the primary side will be broken. My question is that when the primary side is broken by the high input voltage, what will happen on the secondary side—can it be kept safe? Thanks.
Best regards,
Wayne