Other Parts Discussed in Thread: LM2903, INA300, INA381
Hi,
Below is the schematic. Actually, my customer used 3 INA301 with the same circuit, but only one had problem.Just 1A load will cause Alert. the designed over current is 13A, Rlimit is 25K. the shunt res is 7.5mΩ。
From TP1, can observe below waveform through an oscilloscope
From TP2 ,the waveform is as below;
Apparently there was a wing at IN+. and tried to remove the capacitance marked with red box in schematic, the problem has not been solved..
Then found there is a big transformer on the back of the INA301 with problem. and the switch frequency is close to the number in the picture 2[57Khz]
. [below is the transformer, just right behind the INA301], and this is a two-layer PCB design.
My questions are:
(1) any suggestion to the root cause
(2)How to fix this?
(3)Any better device for this case?
Thanks.