Part Number: TLV1805
Hi team,
I'd like to confirm the test condition of figure 22. Maximum Continuous Current vs. Ambient Temperature.
There are some curve when the voltage is 5V, 12V, 21V, 30V, 40V. I think these value is supply voltage. Is it correct?
I also want to confirm the typical output current of TLV1805 is 100mA. Is there any data when 100mA output current vs. Ambient temperature?
Regards,
Yoshi