This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OP07: Functional Block Diagram

Part Number: OP07
Other Parts Discussed in Thread: UA741

Hi E2E,

Good day.

Can you please confirm if the functional block diagram of OP07C/OP07D Precision Op-amp indicated on section 9.2 and UA741 General Op-amp indicated on section 7.2 are the same according to the datasheet?

Thank you very much in advance for your help.

Best regards.

  • Hello Carlo,
    I am moving your question to the group that supports precision amplifiers for a quicker reply.

  • Hi Kirby,

    Do we have updates any updates on this?

    Thank you.
  • Hi Carlo,

    The functional block diagrams shown in OP07C/OP07D Fig. 9.2 and UA741 Fig. 7.2 are the same; however, the diagrams are general purpose in nature and don't necessarily show all the circuit details. Certainly, the OP07C/OP07D much higher electrical performances when compared to the UA741 come about from more advanced processing and circuit techniques not revealed in the functional block diagrams.

    Functionally, the OP07C/OP07D should be able to drop into almost any UA741 application circuit. But note there is one notable pin-out difference between them. The OP07C/OP07D offset control pins are 1 and 8 (pin 5 NC), while for the UA741 they are pins 1 and 5 (pin 8 NC). If the offset control pins are not used and simple left to float on the PC board, then one should be able to plug in the OP07C/OP07D or UA741 and obtain circuit functionality. Do note that the circuit performances obtained will be different due to each Op amp's different levels of electrical performances.

    Regards, Thomas

    Precision Amplifiers Applications Engineering