Part Number: THS4513
Hi
I am trying to test the Aol for THS4513. It is not behaving as expected.
With:
Vsupply: ± 2.5v
+Vin: 30mV
-Vin: -30mV
no feedback resistors.
I get ~± .7v on the ouput; open loop gain of ~24.
Is this right? Where is the 63dB Aol coming from in the datasheet?
Also I currently do not have access to the Texas Instruments website or any of the app-notes or datasheets because my computers security software is malfunctioning. So I will not be able to open any link that is sent.
Thanks
Tony