This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV611: CMVR-temperature curve of LMV611

Part Number: LMV611


I see the following parameters in the data manual of LMV611. I want to know how much CMVR is when the temperature is between 85~125℃. Is there any relevant test data and CMVR-temperature curve?

  • Part Number: LMV611

    I see the following parameters in the data manual of LMV611. I want to know how much CMVR is when the temperature is between 85~125℃. Is there any relevant test data and CMVR-temperature curve?

  • Hello Jace,

    See figure 2, 3, and 4 in the data sheet. It shows the offset for various supply voltage and temperatures. Mathematically interpolating the range between 85C and 125C could be tried, however it would be better to select on op amp that can do V- to V+ over the entire operating temperature range.