Part Number: LM139AQML-SP
Other Parts Discussed in Thread: LM139AQML, LM324
Hi Team,
A customer of mine has a question about the LM139AQML-SP
In the Application Design Guidelines SNOAA35–April 2019 under chapter “5.1 Unused Comparator Connections”, they describe how to connect the unused comparators.
It requires resistors in the input, floating outputs and biasing the inputs.
However in our current designs, the connection of Unused Comparators is done as described in the datasheet LM139AQML - SNOSAH8G:
“All pins of any unused comparators should be tied to the negative supply.”
For us it is important to know if , with the current implementation, there is a risk. Finally needs to modify existing designs?
Our analysis shows, that:
- Connecting the output to the negative supply is not a problem. Supply voltage is 15V.
- Connecting the inputs to the negative supply without resistor should not be a problem. ? Pins are directly connected via short tracks to the negative supply.
- Having no bias voltage, could not be answered by us. Is there a risk of an internal oscillation? Pins are directly connected via short tracks to the negative supply.
I see from this other thread that the LM139AQML-SP does not have internal ESD diodes, so input current limiting would be unnecessary.
https://e2e.ti.com/support/amplifiers/f/14/t/797303
Could you please clarify what the best practice here should be?
Regards
Mihir