Part Number: OPA552
I have the OPA552 opamp in a circuit with a gain of ~6.5. I dropped the resistor values and now I have a clean signal. I have two of these in a circuit and one is used as a simple 40v switch for DC current. Both are driving resistor loads(currently 10Kohm). Both of these opamps are hot to the touch (~80C). I now have a stick-on heatsink. Is it normal for this component to run hot?