We have a TLV3011-EP ( TLV3011AMDBVREP ) where the reference output goes from 1.25v nominal at ambient temperature to about 3.58v when the temperature is less than -40C. We are suspicious as this is our only failure out of about 200 units, and -40C is the lower temperature for the industrial part.
I've read over the thread https://e2e.ti.com/support/legacy_forums/hirel/f/935/p/639438/2386983?tisearch=e2e-sitesearch&keymatch=TLV3011-EP#2386983, and there seems to be a thought that the input V- is sensitive to having ANY positive voltage on it prior the supply voltage coming up. Also there are no clear guidelines on maintaining margin to protect against this behavior as it's not characterized and it varies with temperature.
Our topology is a differential op-amp that that feeds the V- input on the TLV3011-EP. Both amps are powered by the same +5v supply, have the same value bypass caps, and are physically close to each other over a ground plane. The inputs to the diff amp are also powered by the same supply. So the inputs and outputs are at most in sync with the supply as it powers up, but never exceeding the supply.
Is this a bad chip?