Part Number: OPA2188
Other Parts Discussed in Thread: OPA2196, OPA2189, OPA189
Recently i got a strange distortion out of OPA2188. It distorts even earlier then the data sheet specified slew rate limit of 0.8V/us. And additionally distorts not just as slew limit, but actually decreases output signal level much more.
Using a +/-13.5V supply and inputing a 10Vp, 10kHz signal i got following output signal after three OP-Amp stages with OPA2188.
Channel 1: Input Signal, Channel 2: Output Signal after three stages, Channel 4: Output after two stages.
Looking on input of N302.2 shows large ringings during distortion phases:
What is the reason for this and is there a good way to improve/fix it?
Schematic:
Update: OPA2196 looks promising as drop in signal path alternative ... Let's wait for the samples.