Hi everyone,
I have a sine wave going through a circuit of R and C in series. R = 20kohm, C = 300pF. The sine wave signal is 20V pk-pk at 1kHz.
I connect the +in and -in of the INA 129 at the two sides of the resistors. So, the +in reads the sine wave input 20V pk-pk and the -in reads what ever the voltage drop across R.
I leave Rg pins on the INA129 floating (gain = 1 based on the formula provided in the datasheet)
What I see is some drifts at the INA129 output. When I place the heat gun near the circuit, the output signal increases. When I place the heat gun away from the circuit, the output signal decreases.
Is the internal gain of the INA129 temperature dependent? or it is some quirk from my capacitor/resistor?
Thanks,
Khoi Ly