This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7321: Can you help review my VCOM circuit?

Part Number: LM7321


HI 

Would you help review my circuit below, is it ok for -0.21V ~ -3.03V VCOM ? Where VSN is -6.5V. Thanks!

  • Hi PYTsai,

    The circuit should work fine for an input voltage between -0.21V to -3.03V. Also for this application you can also consider using a low-voltage op-amp since you're buffering signals between -0.21V to -3.03V. Low-voltage devices typically have better output swing to rail, if that's something that you're interested in. 

    Best Regards,

    Bala Ravi