This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/OPA548: OPA548 AC Current Regulator

Part Number: OPA548
Other Parts Discussed in Thread: TINA-TI

Tool/software: no

Hi,

Opa548  does it work as an alternating current/voltage regulator?

Like this : +/-5V 1A

  • Mustafa,

    I'm not sure what you mean by saying "alternating current/voltage regulator" but if you mean whether OPA548 can sink and source current then that is correct - since OPA548 has class AB output stage, it can sink/source up to 3A (see below).  Of course, the higher output current requires further output voltage swing from the rail, which is shown in the table below.

    You may simulate +/-5V output with 1A peak current, which requires 5ohm load resistor  - see below output.

    I have attached below Tina-TI schematic you may use for your own simulations.

    Mustafa OPA548.TSC

  • Thank you Marek.

    I didn't see it. That's exactly what I'm looking for.

    Best regard..