Part Number: INA203
What is the maximum delay time for the comparator?
What is the upper limit of the maximum load capacity of the CMP 2 delay terminal?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA203
What is the maximum delay time for the comparator?
What is the upper limit of the maximum load capacity of the CMP 2 delay terminal?
Hello user4395619,
Thanks for posting your questions to the forum.
There should be no upper limit to the maximum load capacity of CMP 2 delay terminal. The datasheet mentions examples where Cdelay =0.2uF and this implies 1 second of delay according to equation 1 of datasheet.
Hope this helps.
Best,
Peter Iliya
Current Sensing Applications