Part Number: LPV802
Hi there
In LPV802 datasheet
http://www.ti.com/lit/ds/symlink/lpv802.pdf
Page-14 has an application circuit information. It shows a potentiostat circuit. & transimpedance amplifier.
This is one of the very few application notes that I have found that has information on this type of circuitry. So, very helpful (thank you very much for sharing this information)
My question is about the component calculation / selection for the resistors & capacitors around potentiostatic circuit (Not the transimpedance amplifier)
The resistors R1, R2 & Cap C1
The datasheet says R1 is to maintain stability due to the large capacitance of the sensor. C1 and R2 form the Potentiostat integrator and set the feedback time constant.
I am trying to figure out a method to calculate these component values OR how the designer came up with the values of
R1 = 10K
R2 = 10K
& C1 = 0.1uF
Although gas sensor manufacturers don't provide the capacitance value for the sensor but roughly say anything from 1mF to 3mF (based on some notes from Alphasense)
So, if we had a sensor of say 1mF and want to use same LPV802 amplifier then how would one calculate these R1, R2 & C1 values (even though the sensor would most likely work if I just use this circuitry), but I would like to understand the underlying methodology to calculate these values!?