Part Number: OPA2277
Does OPA2277 provide single power supply?For example,VCC + is connected to +15V,VCC is connected to GND, can it be used in this way? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2277
Does OPA2277 provide single power supply?For example,VCC + is connected to +15V,VCC is connected to GND, can it be used in this way? Thank you.
Hello,
Yes, the OPA2277 can be powered from a single +15 V supply, V+ = 15 V, V- = 0 V. Note however, that when an Op amp such as the OPA2277 is powered by a single positive supply that the (VCM) Common-Mode Voltage Range is (V–)+2 to (V+)–2, and the output (VO) Voltage Output, RL = 10 kΩ (V–)+0.5 to (V+)–1.2. Thus, with the single +15 V supply VCM becomes + 2 V to +13 V, and Vo becomes +0.5 V to +13.8 V.
These operating conditions must be observed to maintain liner operation.
Regards, Thomas
Precision Amplifiers Applications Engineering