I'm looking for an Audio Amplifier with the following baseline specs, but I'm finding it hard to chose a suitable part.
So, I'm asking the community for help!
My ideal part would be:
- Class D with Stereo or 2.1 Output channels
- 50 W per channel or thereabouts
- I2S (Digitial) input
- 4 (or more) programmable BiQuads for EQ (Or a 5-band EQ)
- I2C Control from a host MCU
The following would be even better but not essential
- Input and output channel mapping
- Preset EQ curves
- Preset crossover settings
- Low THD at full power
Any suggestions?