This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM675: Single Supply?

Part Number: LM675

Hi.

1.- Can LM675 work with single supply?

2.- Which is the minimum supply voltage for single supply? (Can it work with a single supply of +15V?)

3.- I have a LM675 supplied with a dual supply of +/-15. And the LM675 is quite hot even with no current at the output pin. Is this normal?. Note: The component is on the air (not fixed to the PCB and has no heat sink)

Thanks