Part Number: TLV3501
Hi Sir:
I use the high-speed Comp TLV3501. But when I use the DC single input,it can the Vpp=20mV the Device can output the waveform normal。But when I use a pulse single the Vpp must be over 200mV。 Otherwise, the output like oscillation。 And I Add a Feedback capacitance form output to input。But the effect is not ideal