Hello team,
Hope you are doing well. See below customer question;
I am using this part as a buffer in my circuit. It appears the part has a very high leakage at the positive input even though the spec sheet says it has a very high input impedance and very low leakage current. I have attached a snippet of my schematic below. Please note R107 & R108 in my schematic are NOT loaded. I am charging a capacitor (100nF film capacitor) which is connected to the positive input of the op amp as a reference voltage. The negative input is connect to the output for a gain = 1. The voltage source charging the capacitor is then removed and I expect the capacitor to stay charged for a relatively long time (20mV drop > 200 seconds). However, it is discharging very fast. Can someone please explain why this is happening? I selected this part to be low power with a very high input impedance.