This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA381: INA381 output offset issue

Part Number: INA381
Other Parts Discussed in Thread: LM3643,

Hi team,

We face a problem with using INA381A1 to monitor the current on a LED drive LM3643 output. Once there is no current flow thru the LED bus, there is a output offset voltage around 0.568V at INA381 Vout. Even we short the IN+/IN- together and connect to GND, there is still a 0.55V voltage there. The Vout does not connect to anywhere except the CMPIN. We also tried discount to CMPIN but the offset voltage still exist. 

I saw the Vout is able to swing to GND. So it should be not the swing limitation.

Could you provide your comments on what may cause this problem? 

Thanks!

Regards,

Alex