Part Number: LM393
Other Parts Discussed in Thread: TLC372, TLV3702, TLV3402, TLV7032, TLV7011, TLV4041
Hi Team,
We are using LM393D to indicate battery low in our design. Please find our circuit and observations below
During design phase we used 5.1K at R98. So Vref=2.2V.
Now after battery tuning it has to be 2.8V. so, we have replaced R98 with 1.78K.
Note: We gave Hysteresis loop for output stability.
Observations:
Comparator's output is low even when V+=5V (PIN 3) and V-=2.8V (PIN 2)
We tried without Hysteresis loop also(without R117), but the result is same - Output is low.
I request you to share your input on the design and the above issue.
We are awaiting for your response
Thanks & Regards,
E.Rohini