This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA694: OPA694

Part Number: OPA694


Dear TI team:

    My customer used OPA694 for signal amplification. The previous power supply is ±5V, the output is normal, and when they change power to +3.3V and -5V, the output level is lower than before, why is it happen?

   And if customer used +4V and -5V, can OPA694 output normal? 

   What data are required from customers? The customer is not very willing to provide some information, the input is changing, is pulse.

   Thanks!

Regards!

Eric Shen