Part Number: LM139
Other Parts Discussed in Thread: TLV7011
If I’m holding one input at the midpoint by two identical resistors. Like two 1k resistors so the reference level input is 3.3/2 = 1.65V and the other input will swing up and down 0v to 3.3v while Vcc=3.3V, can we guarantee across the temperature range that the output will also flip correctly accordingly?