Part Number: AMC1301
Other Parts Discussed in Thread: ISO224, AMC1311
Hello,
i want to design a +/-10V input with +/-8V linear inputrange of the AMC1301. Themaximung current of the source is 5mA.
The tolerance of the input must be very low and the bandwidth shoud be a around 50-100kHz.
In the datasheet of the AMC1301 is the following text about gain errors:
1. Is it possible to compensate the Gain error according formula (1) by calculating the parallel resistence of the "shuntresistor" and the input resistance of the AMC1301?
2. Is it also possible to compensate the Gain error according formula (2) by using a higher value of R3?