Part Number: LMH5401
Other Parts Discussed in Thread: LMH6554, ADS54J54
Hi,
I’m working on a 4 channel FMC converter board design that strictly requires DC coupled signal path through out. The input signal range is +/-0.5V single ended, so I have to use a diff amp as input stage. Most of the high speed ADCs including ADS54j54 have a rather high Vcm around 2V but most of high speed diff amps like LMH5401 have rails limited to +/-2.5V. This makes connecting Vcm output of the ADC to Vcm input of the diff amp impractical at best because the output of the diff amp will go too close to the positive rail (even with G=0dB) resulting in unacceptable harmonic distortion. I was considering LMH6554 which can be run with +/-5V rails but the part has too much HD2 and HD3 at higher frequencies (above 100MHz) degrading ADC linearity as a result. Is there anyway round this problem? Any suggestion device-wise, diff amp or ADC that works better together?