Other Parts Discussed in Thread: OPA1612
Hello,
I have a question about the Harmonic distortion with TINA, take OPA1612 for example, the Harmonic distortion is 3.886% when using inverting input, while the harmonic distortion is 0.0002% when using non-inverting input. My personal understanding is opposite because the inverting input could not encounter input crossover distortion due to its Vcm doesn't change Vcm=0, so the Harmonic distortion of inverting input should less than non-inverting input, but the results of TINA is opposite.
Best regards
Kailyn