Other Parts Discussed in Thread: LMH6518
Hi,
I am using LMH6518 EVM to amplify the signal.
I am providing PAM3 signal as an input & measuring output of amplifier.
There is some eye opening at input side (eye height is 26mVpp) but output of amplifier gets noisy (i.e. there is no eye opening at all).
I have set gain of 18.8dB.
Below are the images for reference.
Image1: Input of amplifier
Image2: Output of amplifier
Can you please provide any suggestion on it?
Regards,
Vishal Dhanani